EtherCAT Features
- 1000 I/Os in 30 µs.
- Optionally twisted-pair cable or optical fiber.
- Optimum vertical integration (thanks to Ethernet Ethernet is a large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs) and Internet technologies).
With EtherCAT, the costly Ethernet star topology is replaced with a simple line structure - no expensive infrastructure components are required.
- Optionally, EtherCAT can be wired in the classic way using switches, to integrate other Ethernet devices.
- Where other real-time Ethernet approaches require special connections in the controller, for EtherCAT, very cost-effective standard Ethernet cards suffice.
EtherCAT is Versatile
These communication connections are supported (see image):
- Master to Master
- Master to Slave
- Slave to Slave
Figure 9-52: Versatile Network Architecture
Safety over EtherCAT is Available
- EtherCAT makes Ethernet down to the I/O level technically feasible and economically sensible.
- Outstanding features of this network include:
- Full Ethernet compatibility.
- Internet technologies (even in simple devices).
- Maximum utilization of the large bandwidth In computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz offered by Ethernet.
- Outstanding real-time characteristics at low costs.